Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the lug temperature rating for the PQ Fusible Plug-In Units?
Issue:
Lug temperature rating for the PQ Fusible Plug-In Units

Product Line:
Busway

Environment:
Products sold and used in North America

Resolution:
Above 100A (101A or more) the lugs are rated at 75 degrees Celsius
1000A and less, the lugs are rated 60 degrees C.  75 degrees C insulated conductors can be used but the conductors have to be sized per the 60 degrees C table in the NEC.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings