Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the handle padlock attachment for padlocking HOM breakers in the ON or OFF position?
Issue:
What is the handle padlock attachment for padlocking HOM breakers in ON or OFF position?

Product Line:
Homeline circuit breakers

Resolution:
For padlocking 1 pole, standard Homeline breakers in the ON or OFF position:
  • HOM1PA
For padlocking 2 pole, standard Homeline breakers in the ON or OFF position:
  • HOM2PALA for breakers up to and including 70 A
  • HOM2PAHA for breaker amperages of 80 to 125 A
  • HOM2PAVHA for breaker amperages of 150 to 200 A
For padlocking ground fault and arc fault breakers in the ON or OFF position:
  • HOMELEC1PA for locking single pole HOM-CAFI, HOM-PCAFI, HOM-EPD, HOM-GFI, HOM-DF, and HOM-PDF breakers.
  • HOMELEC2PALA for locking two pole HOM-CAFI, HOM-EPD, and HOM-GFI breakers.

Schneider Electric Canada

Attachment(s)
HOM Handle Accessories.pdf [119.93 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings