Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why do we set in a thermal overload relay in star-delta starters at 58% of the <br />rated motor current?<br />
Product Line:

NEMA style Overload Relays

Resolution:
Because of the way the connection is made in RUN(delta) mode, the full load current is shared across the 1M and 2M contactors. Because of this, the thermal units must be sized at 58% of the motor full load current rating.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings