Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the 8903 lighting contactors fully rated?
Issue:
Are the 8903 lighting contactors fully rated?

Product Line:
Digest 177 Section 16 : Nema and Definite Purpose and Starters

Environment:
North American Products

Cause:
Are the 8903 lighting contactors fully rated?

Resolution:
Yes. All Class 8903 Type ``S`` lighting contactors are fully rated for tungsten, ballast and resistive applications. Therefore the contactor may be used to control a load up to its full nameplate rating. Derating of the contactor is not necessary as is standard practice with circuit breakers and fuses.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings