Issue:
Product Design Feature
Product Line:
QO and Homeline load centers
Cause:
Clarifying lug wire range
Resolution:
The LK70AN will accept a #12 - 2 AWG aluminum or #14-4 AWG copper wire.
The LK100AN will accept a #6 - 2/0 AWG AL or CU wire.
The LK125AN will accept a #14 - 2/0 AWG aluminum or copper wire.
The LK150AN will accept a #2 - 3/0 AWG aluminum or copper wire.
The LK225AN will accept a #4 AWG - 300 kcmil aluminum or copper wire. (For use in Series S, 150 - 225A QO load center OR Series S03 and below 150-225 A Homeline load centers
The LK225ANHOM will accept a #4 AWG - 300 kcmil AL/Cu wire. For use ONLY in Series S04, 150 -225A Homeline load centers
Product Design Feature
Product Line:
QO and Homeline load centers
Cause:
Clarifying lug wire range
Resolution:
The LK70AN will accept a #12 - 2 AWG aluminum or #14-4 AWG copper wire.
The LK100AN will accept a #6 - 2/0 AWG AL or CU wire.
The LK125AN will accept a #14 - 2/0 AWG aluminum or copper wire.
The LK150AN will accept a #2 - 3/0 AWG aluminum or copper wire.
The LK225AN will accept a #4 AWG - 300 kcmil aluminum or copper wire. (For use in Series S, 150 - 225A QO load center OR Series S03 and below 150-225 A Homeline load centers
The LK225ANHOM will accept a #4 AWG - 300 kcmil AL/Cu wire. For use ONLY in Series S04, 150 -225A Homeline load centers
Released for: Schneider Electric Canada