Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: What filler plate is used to fill unused branch circuit openings in a Homeline load center and how does it get intsalled?
Issue:
Product Design Features

Product Line:
Homeline Load Centers

Resolution:
The filler plate for use in the Homeline load centers is part number HOMFP.  The part number HOMFP are the ONLY filler plates to be used for the Homeline load centers to fill a branch breaker opening in the deadfront trim when a twistout has been removed and no branch breaker will be installed in that position. The HOMFP will contain 5 filler plates in the package.
NOTE: the filler plate is plastic and approximately 1" wide x 2.56" long, BUT this is the ONLY filler plate available for Homeline Load Centers.

The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.

A PDF copy of the complete instructions is attached below the video.

Danger label

Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
1) Once all Safety steps are followed, begin the installation of the Branch Breaker opening filler plate by following the instructions.
2) Install the filler plate from the front of cover by pressing into place as shown in the instructions.
NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

Schneider Electric Canada

Attachment(s)
HOMFP Instructions.pdf [91.24 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings