Issue:
What is the difference between Class 2510 Type K*1 and Class 2510 Type K*5?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
2510 type K manual switches
Resolution:
Horsepower ratings as follows:
What is the difference between Class 2510 Type K*1 and Class 2510 Type K*5?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
2510 type K manual switches
Resolution:
Horsepower ratings as follows:
| Maximum HP Ratings | ||||
| Manual Switch | 115V | 230V | 460V | 575V |
| K*1 | 2 | 2 | 3 | 3 |
| K*2 | 2 | 3 | 7.5 | 10 |
Released for: Schneider Electric Canada