Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the secondary ring nut available in metal for the 9001K Selector Switch?
Issue:
Replacement metal ring nut for 9001K Selector Switches

Product Line:
Push Button and Operator Interface

Environment:
9001K Selector Switches

Cause:
The black insert plastic ring in9001KS53B selecto switch keeps breaking.  Would like to see if there is one in metal.

Answer:
No, it's not available in metal.  The replacement part number is 9001SK46  (K46 is no longer available).

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings