Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the mounting hole diameter for a 9001J ?
Issue:
What is the size of the hole for the 9001J to fit?

Product Line:
Push Buttons and Operator Interface

Environment:
9001J Operators

Resolution:
Mounting diameter is 11/16`` or 17.5mm

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings