Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the wire ranges for the neutral and ground lugs provided in the Q22200NS, Q22200NRB, Q23225NF, Q23225NS, or Q23225NRB circuit breaker enclosures?
Issue:
Product Feature

Product Line:
Circuit Breaker Enclosure

Resolution:
The neutral lugs will accept (2) #4 AWG  - 300 kcmil Al/Cu (1 incoming and 1 outgoing).
There are also two terminals for service ground wires, if used as service equipment, capable of #14 AWG - #1/0 AWG Al/Cu.
These enclosures use Q frame breakers, which accept #4 - 300 kcmil Al/Cu.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings