Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the replacement mechanical interlock for an 8736SDO2?
Issue:
What is the replacement mechanical interlock for an 8736SDO2?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S contactors or starters Class 9999 Accessories

Resolution:
9999SM6. This interlock can be used on any 2 pole or 3 pole NEMA Size 2 Type S contactor or starter combination for horizontal mounting.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings