Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you get spring terminals on a LC1D contactor?
Issue:
Spring Terminals on a LC1D Contactor

Product Line:
IEC Contactors

Environment:
Tesys D Contactors

Cause:
Product Specification

Resolution:
Spring terminals are available on D-Line contactors when specified at the time of order only.  For spring terminals versions of LC1D09– LC1D65A, add 3 to the catalog number prior to adding the voltage code (for example, LC1D12G7 becomes LC1D123G7 and LC1D40AG7 becomes LC1D40A3G7. Note that 40–65 A spring terminals are only on the control terminations and not on power terminations).

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings