Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the standard flange and diaphragm material used on a 9013F pressure switch?
Product Line:
9013 pressure switches

Resolution:
The flange is made of Cold steel, plated with zinc iridescence chromate
The diaphragm is made of Buna N rubber. Note for a brief period they were using a white TPE Arnitel EL550 plastic. You can tell the difference by looking at the color of the diaphragm. The Buna N is Black and the TPE Arnitel is white.

Schneider Electric Canada

Attachment(s)
9013 Troubleshooting 9013DB0701.pdf [100.93 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings