Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does a ZB2BV6 or a ZA2BV6 include a lamp?
Issue:
Identify if a bulb needs to be ordered separately from light module.

Product Line:
22mm Light Modules for Push Buttons

Environment:
Push Buttons and Operator Interface

Resolution:
No, lamp is not included unless voltage code suffix is attached, such as ZB2BV624V includes a 24V lamp, a ZB2BV6120V includes a 120v lamp, etc.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings