Issue:
Red reset bar on the 8536SE* starter or 9065SDO** overload relay
* - Represents any enclosure designation. ** - Represents digits 11 through 14.
Product Line:
NEMA Starters
Environment:
Class 8536 Type S starters
Resolution:
The replacement red reset bar is part number 31075-008-01.
This also applies to all 8538SE, 8539SE, 8606SE, 8630SE, 8640SE, 8702SE, 8736SE, 8738SE, 8739SE, 8810SE, 8903SE, 8940SE, and 8941SE devices.
Red reset bar on the 8536SE* starter or 9065SDO** overload relay
* - Represents any enclosure designation. ** - Represents digits 11 through 14.
Product Line:
NEMA Starters
Environment:
Class 8536 Type S starters
Resolution:
The replacement red reset bar is part number 31075-008-01.
This also applies to all 8538SE, 8539SE, 8606SE, 8630SE, 8640SE, 8702SE, 8736SE, 8738SE, 8739SE, 8810SE, 8903SE, 8940SE, and 8941SE devices.
Released for: Schneider Electric Canada