Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are "mousetrap type" I-Line series 1, NEHB 600A Series E1, and NQOD 400A and 600A Series E1 trims clips?
Issue:
What is the catalog number for a trim clamp that has a gray plastic washer-like part in front with a slot head screw through its center, and in back a mechanism similar in appearance to half of an old-fashioned spring clothespin?

Product Line:
Panelboards

Environment:
NQOD, NEHB and I-Line Panelboards

Cause:
N/A

Resolution:
Use a LP9501 ( 1 per kit).

Schneider Electric Canada

Attachment(s)
LP9501.JPG.jpg [36.95 KB]
Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings