Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are Replacement Parts Available for Pre-series 8502 / 8536 devices?
Issue:
Replacement components / rebuild kit may be needed for pre-series device 8502 / 8536

Product Line:
NEMA Class 8502 /8536 Type S

Environment:
NEMA Contactors and Starters

Resolution:
For pre-series 8502 / 8536 Type C, B, D, E, F, G, H, J, the replacement parts had all been obsolete. This design has been obsolete since the late 1960`s. Due to low demand and the high cost of manufacturing, the replacement contact kits are obsolete. If a complete replacement device is required or desired, please use the Competitive Cross Reference tool.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings