Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is ZB2BZ91 and ZB2BZ92 time delay contact block ON delay or OFF delay?
Issue:
ZB2BZ91 and ZB2BZ92 time delay type

Product Line:
Harmony 22mm Push Buttons

Environment:
XB2/XA2 22mm Push Buttons

Cause:
Confirm the action of 2 contact blocks before installing into application.

Resolution:
Both contact blocks are ON DELAY. ZB2BZ91 is a 30 second delay and ZB2BZ92 is 180 second delay. Both of these blocks are obsolete.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings