Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can an LA11021 shunt trip be installed on an LA36400 breaker series 3?
Issue:
Can we field install a shunt trip for the LA36400 Series 3 breaker?

Product Line:
LA frame Circuit Breakers

Environment:
Products sold in North America

Resolution:
The field installable accessories, including Shunt Trip, will only work on Series 4 breakers.
There are no field installable accessories available for the Series 3 breakers.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings