Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the solid state overload relays ambient compensated?
Issue:
Are the Class 9065 motor logic solid state overload relays ambient compensated?

Product Line:
Nema and Definite Purpose and Starters

Environment:
Motor Logic Overload Relay

Cause:
Needs to verify if the Class 9065 solid state overload relays ambient compensated.

Resolution:
No, these overloads are ambient insensitive which means as long as the overloads are used within the rated temperature range (-25 to 70 degrees Celsius) the ambient will have no affect on the trip curve.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings