How can we help you today?

Can the Class 2510 Type K switches be used on 50 hertz applications?

Issue:
Are the 2510K Manual switches suitable to be used on 50Hz applications?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
NEMA Manual Starters and Switches

Resolution:
All testing and evaluation of these devices are performed at 60HZ. The device has no control coil so there is no problem in this area. In consideration of the load the power contacts would see, they are horsepower rated and follow the tables in UL 508 for determination of current at specific horsepower and voltage levels. As long as the horsepower rating and/or maximum continuous current rating (30 amps) is not exceeded, the devices should function acceptably.

Schneider Electric Canada
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
Start your sales inquiry online and en expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings