Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the catalog numbers for the fuse clip kits for D10S4?
Issue:
Fuse clip kits for D10S4

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Class D10 Disconnect Switches

Resolution:
61-100 amp, 600 volts, H or K fuse clip kit is D12F63
101-200 amp, 600 volts, H or K fuse clip kit is D12F64
101-200 amp, 600 volts, R fuse clip kit is D12FR64
101-200 amp, 600 volts, J fuse clip kit is D12FJ4
101-200 amp, 250 volts, H or K fuse clip kit is D12F24
101-200 amp, 250 volts, R fuse clip kit is D12FR24
201-400 amp, 250 volts, H and K fuse clip kit is D12F25 (cannot be used with service entrance rated switch)
201-400 amp, 250 volts, R fuse clip kit is D12FR25 (cannot be used with service entrance rated switch)
201-400 amp, 600 volts, H and K fuse clip kit is D12F65 (cannot be used with service entrance rated switch)
201-400 amp, 600 volts, R fuse clip kit is D12FR65 (cannot be used with service entrance rated switch)
201-400 amp, 600 volts, J fuse clip kit is D12FJ5 (cannot be used with service entrance rated switch)

FYI: D10S4 Disconnect Switch was discontinued in June 2021

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings