Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the wire size for the neutral on a C60H RCBO, part number 26858?
Issue:
RCBO Wire size

Product Line:
Circuit Breakers

Environment:
Multi-9 RCBO

Resolution:
Neutral cable section: up to 32A = 2.5 mm; for 40 and 45A =4 mm (40A not sold under Square D brand)
Ground cable section : 0.75 mm?

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings