Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the current transformer (CT) ratio for the overload relay on the Class 8536 Type SH starter?
Issue:
Identifying current ratio of the current transformer in a NEMA size 6 starter

Product Line:
NEMA starters

Environment:
Products sold and used in the United States

Cause:
Identifying current ratio for the current transformer in a size 6 starter

Resolution:
For bimetallic and melting alloy 800:5, for Solid State 600:5.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings