Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are LC1DREQ3831G * and LC2DREQ3832G *? ( * = Could be 1, 2, 3, 4, 5 or 6.)
Issue:
Is LC1DREQ3831G* a valid part number?

Product Line:
Contactors and Starters IEC

Environment:
Tesys D Contactors

Resolution:
These are special contactors for General Motors, basically they are LC1/LC2 40 amp through 150 amp contactors with auxiliary contacts which are locked into place using a wedge. If additional information is required, contact the Raleigh Product Support Group.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings