Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do the Class 9065 Type SP Motor Logic Plus Overload Relays provide ground fault detection?
Issue:
Do solid State overload relays provide ground fault detection?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment
9065 Solid state overload relays

Resolution:
Yes, this solid state overload relay calculates ground fault condition based on a summation of the three phase current. It is adjustable from 0.15 times minimum over current setting to 0.20 times the maximum over current setting. Please note that the device is for equipment protection and in no way should be used as people protection. Additionally, this solid state overload is not intended to take the place of branch circuit protective devices, such as circuit breakers or fuses.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings