Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to use the 9001BG*** control station contacts at 24VAC?
Issue:
Checking on the possibility to use the 9001BG*** control station contacts at 24VAC.

Product Line:
9001B Control Stations

Environment:
Control Stations and Enclosures

Resolution:
Yes, as long as the current rating is not exceeded.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings