What is the replacement handle operator part number for the Class 9421 Type NC* and Type ND* disconnect switch?
Issue:
Handle operator part number for the Class 9421 Type NC* and Type ND* disconnect switch
Product Line:
Class 9421 Circuit Breaker Operating Mechanism
Environment:
Operating Mechanisms for Circuit Breakers
Resolution:
The switch is supplied as standard with 9421NW2, red operator and yellow legend plate. There is an optional black operator which is 9421NW2B.
Handle operator part number for the Class 9421 Type NC* and Type ND* disconnect switch
Product Line:
Class 9421 Circuit Breaker Operating Mechanism
Environment:
Operating Mechanisms for Circuit Breakers
Resolution:
The switch is supplied as standard with 9421NW2, red operator and yellow legend plate. There is an optional black operator which is 9421NW2B.
Released for: Schneider Electric Canada