What are the permissible mounting orientations for NEMA motor starters?
Issue:
Mounting orientations for NEMA motor starters
Product Line:
Nema and Definite Purpose and Starters
Environment:
Contactors and Starters
Cause:
Needs the permissible mounting orientations for NEMA motor starters.
Resolution:
All devices must mount in the vertical plane. For NEMA sizes 00 - 4, the device may be mounted so that it is rotated 90 degrees clockwise or counterclockwise. For NEMA sizes 5 and above, the device must remain in the vertical position.
Mounting orientations for NEMA motor starters
Product Line:
Nema and Definite Purpose and Starters
Environment:
Contactors and Starters
Cause:
Needs the permissible mounting orientations for NEMA motor starters.
Resolution:
All devices must mount in the vertical plane. For NEMA sizes 00 - 4, the device may be mounted so that it is rotated 90 degrees clockwise or counterclockwise. For NEMA sizes 5 and above, the device must remain in the vertical position.
Released for: Schneider Electric Canada
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.