Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What Are the environment ratings for the 9001 Assembled Control Stations?
Issue:
What are the UL/NEMA environment enclosure rating information for 9001KYK, 9001KYSS control stations?

Product Line:
Pushbutton and Control Stations

Environment:
Class 9001 Control Stations

Resolution:
9001KYK* - UL types 1,3,4 & 13 and NEMA types 1,3,4 & 13
9001KYSS* - UL Types 1, 3, 4 and 13/NEMA 1, 3, 4 and 13—Stainless Steel (304)
9001KYSK* - UL Types 1, 3, 4. 4X and 13/NEMA 1, 3, 4, 4X and 13—Stainless Steel (304)
9001SKY* - UL Types 1, 3, 4. 4X and 13/NEMA 1, 3, 4, 4X and 13—Polymeric (Plastic)
9001KYG* - UL Types 1, 3, 4 and 13/NEMA 1, 3, 4 and 13 Die Cast Zinc Enclosures with Integral Guard

Note: 9001KYK223,  9001KYK322, 9001SKY223, 9001SKY222, 9001SKY122 have sealed contacts and are also UL listed for use in areas classified as Class II Division 2, Group G and Class III.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings