Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the short circuit rating of the Integral Starters?
Issue:
Reference SCCR information for Old Integral Starter

Product Line:
Contactors and Starters

Environment:
Obsolete Integral Starters

Resolution:
42kA up to 480 volts. However these devices are UL Listed as UL508 and not UL508E motor controllers and therfore a short circuit protective device must be supplied upstream.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings