How can we help you today?

Is there grounding means supplied with the Class 8538 Type S____ NEMA size 0 through NEMA size 2 combination starters?

Issue:
Is ground connection provided in Combination starters sizes 0-2?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S combination starters

Resolution:
Yes, ground connection(s) are provided as standard.