Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is an additional neutral lug or equipment ground lug, available for use when a QO2150, QO2175 or QO2200 branch circuit breaker, or QO2225SL sub-feed lug kit is used in a QO single-phase load center?
Issue:
Product accessories

Product Line:
Homeline load centers

Cause:
Application

Resolution:

A neutral lug kit, LK225AN, is provided with these branch circuit breakers, for field installation on the load centers neutral bar. In most applications, a standard equipment ground bar will be able to terminate the circuit's equipment ground conductor. If an additional equipment ground lug may be required, order LK100AN separately, for field installation on a standard equipment ground bar.
NOTE: These breakers can be applied only in Square D SINGLE PHASE QO load centers. DO NOT USE IN Square D THREE PHASE QO load centers or other manufacturers' load centers or panelboards. See the Instruction Sheet provided with the circuit breaker or sub-feed lug kit for further mounting restrictions that may apply regarding mounting these devices or adjacent branch circuit breakers.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings