Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Will the indoor busway (NEMA 1) directly connect to the outdoor busway (NEMA 3R)?
Issue:
Connect Indoor busway (NEMA 1)directly to the outdoor busway (NEMA 3R)

Product Line:
Busway

Environment:
Products sold and used in North America

Resolution:
No. The ends are different on these two styles of busway.
When designing the busway and working with the local distributor or local Schneider Electric sales office, the manufacturing plant will build the section of outdoor busway that transitions indoors to include an indoor connector on the indoors end.  The outdoor busway device will be designed on one end to transition to indoor busway on the section that is indoors.  No special connector required.

See video below for reference:

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings