Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a NEMA 4 stainless steel enclosure available for the QBL, QDL, QGL, and the QJL circuit breakers?
Issue:
Is there an available Stainless Steel Enclosure for Q Frame Breakers?

Product Line:
Molded Case Circuit Breaker Enclosures

Resolution:
No, there is no option for a NEMA 4 or 4X enclosure for the Q frame breakers.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings