Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is required to convert Class 9422 Type TDF60 from 60 amp 250 volt or 30 amp 600 volt to 60 amp 600 volt fuse clips?
Issue:
60A 600V fuse clip conversion kit on 9422TDF60

Product Line:
Disconnect switches and operating mechanisms

Environment:
9422T Disconnect switches

Resolution:
Fuse clip conversion kit is 9422TD63.

If the conversion also requires Class R fuse clips, order one adapter kit Catalog Number RFK06H is required in addition to the conversion kit.
Notes:
1. Form Y157 means this kit will have copper lugs on the fuse base assembly.
2. This kit will not work on the 9422 TEN10, TEF10, TEF13 (100A) disconnect switches.
The following switches can be converted to 60A 600V fuse clips:
1. Class 9422 Type TCN30 (30A non-fusible)
2. Class 9422 Type TCF30 (30A fusible with 30A 250V fuse clips)
3. Class 9422 Type TCF33 (30A fusible with 30A 600V or 60A 250V fuse clips)
4 Class 9422 Type TDN60 (60A non-fusible)
5. Class 9422 Type TDF60 (60A fusible with 60A 250V or 30A 600V fuse clips)

Attached is the parts for the kit and mounting hole for the conversion.

Schneider Electric Canada

Attachment(s)
9422TD63.JPG.jpg [63.42 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings