Issue:
Add 2 quick connects per terminal (total of four) on 8910,8911,8965 on Type DP,DPS,DPR,DPA Contactors
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
DP/DPA Contators
Cause:
Confirming if there's an option for (4) quick connects per terminal on Class 8910 Type DP or Type DPA definite purpose contactors.
Resolution:
Yes, use factory modification form Y247. This will add 2 additional quick connects per power terminal. This modification will provide a total of four connectors per power terminal, however it does not provide any additional control coil terminal connectors.
Add 2 quick connects per terminal (total of four) on 8910,8911,8965 on Type DP,DPS,DPR,DPA Contactors
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
DP/DPA Contators
Cause:
Confirming if there's an option for (4) quick connects per terminal on Class 8910 Type DP or Type DPA definite purpose contactors.
Resolution:
Yes, use factory modification form Y247. This will add 2 additional quick connects per power terminal. This modification will provide a total of four connectors per power terminal, however it does not provide any additional control coil terminal connectors.
Released for: Schneider Electric Canada