Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a SU3040M200R, Series 002?
Issue:
Repair parts list for SU3040M200R

Product Line:
CSEDs

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field replaceable:
Meter Cover Assembly - 4053442852
Meter Cover Assembly Mounting Screw - 4020513001K (contains 10 screws, but only one is required)
Meter Sealing Ring - 2920910001
Main Breaker Cover Assembly - 4053446553 (includes metal cover with integral thermoplastic cover)
Main Breaker Cover Sealing Screw - X1299 Screw and 2361502101 Mylar Washer
Main Breaker - QOM2200VH
Utility Pullbox Cover - 40534-381-52 (includes hinges and utility sealing tab)
Utility Pullbox Cover Sealing Screw - X1299 Screw and 2361502101 Mylar Washer
Utility Pullbox Cover Mounting Rivets - (4) 2430315290
Meter Base Assembly - 4053446152 (includes meter base, line and load side meter jaws, meter jaw blade guides, and load side connector busbars)
Meter Jaw - (4) 7329794850 (included in meter base assembly)
Meter Jaw Blade Guide - (4) 4052761901 (included in meter base assembly)
Line Side (Utility) Phase Lugs - (2) 4025116251, Lug Mounting Keps Nuts (2) 2342702000
Line Side (Utility) Neutral Lug - 4025116051, Lug Mounting Keps Nut 2342702000
Load Center Cover - 4053439153 (includes integral interior deadfront trim)
Load Center Cover Mounting Screws - 4020513001K (contains 10 screws, but only 7 are required)
Load Center Interior Assembly - 4055842550 (does not include load center interior main phase lugs nor (3) larger branch neutral lugs attached to the branch neutral bar; does include load center interior main neutral lug)
Load Center Interior Mounting Screws - (7) 4020510001
Load Center Interior Main Phase Lugs - (2) 4025102451, Lug Mounting Keps Nuts - (2) 2342702001
Load Center Interior Larger Branch Neutral Lugs (attached to branch neutral bar) - #1/0 CU/AL AWG Lug (1) 4025130250 and #4 CU (#2 AL) AWG Lug (2) 4025130450
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings