Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an SC1624M100S, series M01?
Issue:
What are the replacement parts for a SC1624M100S Series M01?

Product Line:
Metering

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field replaceable:
Meter Cover - 4056161350
Meter Cover Mounting Screws - 4020513002K (contains 10 screws; only two screws required)
Meter Sealing Ring - 2920910001
Utility Pullbox Cover - 4056172250 (includes latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover - 7329401401
Load Center Cover Hinges - (2) X2983
Load Center Cover Hinge Mounting Screws (2) 2159414081
Dead Front Interior Trim - 4056168402
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only one screw required)
Load Center Interior - 4056170150 (main breaker not included)
Load Center Interior Mounting Screws - (9) 2153217161
Main Breaker - HOM2100
Meter Base Assembly - 4056223250 (includes meter base with the right, load side meter jaw, blade guide, and L-shaped connector assembled to the meter base)
Meter Jaw - (4) 7329794850
Meter Jaw Mounting Bolt - (4) 2271020242
Meter Jaw Mounting Keps Nut - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Line Side Phase Lugs - (2) 4025102451
Line Side Phase Lugs Mounting Bolt - (2) 2271020242
Line Side Phase Lugs Mounting Keps Nut - (2) 2342702001
Line Side Neutral Lug - LK100AN
Closing Plate - (2) ACP
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings