Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the RC816D200CH, series 002?
Issue:
Repair parts

Product Line:
CSED

Resolution:
Rainproof Cap - 4056115803
Rainproof Cap Mounting Screws - (2) 2142717161
Meter Cover Assembly - 4056143052 (includes latch)
Load Center Cover Assembly - 4056128052 (includes hinges)
Load Center Cover Mounting Rivet - (4) 2430315290
Dead Front Interior Trim - 4056114503
Dead Front Interior Trim Mounting Screw - 4020513001K (this kit contains 10 screws, but only one is required to mount the interior trim)
Load Center Interior - 4056133352 (does not include main breaker or secondary main breaker mounting base; includes feed-thru lugs)
Load Center Interior Mounting Screws - (7) 2153217161
Main Breaker - HOM2200
Main Breaker Retaining Hardware - 4056132701 (hold down strap that straddles across the main breaker), 4056152501 (clamp), 4056152601 (spacer), and 2159417721 (screw)
Feed-Thru Phase Lug Assembly (Left) - 4056133252
Feed-Thru Phase Lug Assembly (Right) - 4056133152
Feed-Thru Phase Lug Assemblies Mounting Keps Nut - (2) 2342702000
Feed-Thru Neutral/Ground Lug - 4025114550 (double barrel lug)
Feed-Thru Neutral/Ground Lug Mounting Nut - 2342702200
Secondary Main Breaker Base Assembly- 4055841752
Secondary Main Breaker Base Assembly Mounting Screws - 2153217161
Meter Base Assembly - 4056149752 (includes load side lugs, meter jaws, and horn bypasses; does not include load side meter jaw blade guides)
Meter Jaw - (2) 7329794850 (load side meter jaws are included in the meter base assembly)
Meter Jaw Mounting Keps Nut - (2) 2342702001 (load side meter jaw mounting keps nuts are included in the meter base assembly)
Meter Jaw Blade Guide - (4) 4052761901
Fifth Jaw Assembly - 4052729550
Fifth Jaw Assembly Mounting Screw - 2153217161
Line Side Horn Bypass - (2) 4056150901 (line side horn bypasses are included in the meter base assembly)
Line Side Phase Lugs - (2) 4025116051
Line Side Phase Lugs Mounting Carriage Bolts - (2) 2271020242
Line Side Phase Lugs Mounting Keps Nuts - (2) 2342702000
Line Side Neutral Lugs - (2) 4025116051
Line Side Neutral Lugs Mounting Keps Nuts - (2) 2342702000
Service Ground Lug - 4025102451
Service Ground Lug Mounting Keps Nut - 2342702001
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings