Issue:
Product Design Features
Product Line:
Circuit Breaker Enclosure
Resolution:
NOTE: For the Video a J250S enclosure was used, but the ground kits will install the same on the other enclosures.
In all the H150_ and J250_ Enclosures, for both 2 and/or 3-pole circuit breakers from 15Amp to 150Amp the equipment ground kit is part number PKOGTH150. This kit contains two lugs, the mounting hardware, ground terminal labels and wire size/torque labels. The lugs will accept (1) #14 AWG - #2 Al/Cu ground wires. (See below attached a copy of the current Installation instructions for this kit)
In all the J250_ Enclosures, for both 2 and 3-pole circuit breakers from 150Amp to 250Amp the equipment ground kit is part number PKOGTJ250. This kit contains two lugs, the mounting hardware, ground terminal labels and wire size/torque labels. The lugs will accept (1) #6 AWG - 300kcmil Al/Cu ground wires. (See below attached a copy of the current Installation instructions for this kit)
NOTE: MAKE SURE TO VERIFY THE PKOGTH150 or PKOGTJ250 KIT CAN BE USED IN THE SPECIFIC CATALOG NUMBER IT IS BEING INSTALLED IN. Because, the kits are used in several different circuit breaker enclosures.
The featured video is ONLY to supplement the INSTRUCTIONS that come with each kit.
PLEASE make sure to read and follow the instructions that come with each PK ground bar kit and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.

Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
Once all Safety steps are followed, begin the kit installation by following the instructions that come with the kit.
Product Design Features
Product Line:
Circuit Breaker Enclosure
Resolution:
NOTE: For the Video a J250S enclosure was used, but the ground kits will install the same on the other enclosures.
In all the H150_ and J250_ Enclosures, for both 2 and/or 3-pole circuit breakers from 15Amp to 150Amp the equipment ground kit is part number PKOGTH150. This kit contains two lugs, the mounting hardware, ground terminal labels and wire size/torque labels. The lugs will accept (1) #14 AWG - #2 Al/Cu ground wires. (See below attached a copy of the current Installation instructions for this kit)
In all the J250_ Enclosures, for both 2 and 3-pole circuit breakers from 150Amp to 250Amp the equipment ground kit is part number PKOGTJ250. This kit contains two lugs, the mounting hardware, ground terminal labels and wire size/torque labels. The lugs will accept (1) #6 AWG - 300kcmil Al/Cu ground wires. (See below attached a copy of the current Installation instructions for this kit)
NOTE: MAKE SURE TO VERIFY THE PKOGTH150 or PKOGTJ250 KIT CAN BE USED IN THE SPECIFIC CATALOG NUMBER IT IS BEING INSTALLED IN. Because, the kits are used in several different circuit breaker enclosures.
The featured video is ONLY to supplement the INSTRUCTIONS that come with each kit.
PLEASE make sure to read and follow the instructions that come with each PK ground bar kit and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.
Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
Once all Safety steps are followed, begin the kit installation by following the instructions that come with the kit.
Released for: Schneider Electric Canada