Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the trim clamp for pre-1986 HCM, HCW, and the HCWM series 1 and 2 for the I-line panel cover?
Issue:
Trim clamp part number for  HCM, HCW, and the HCWM series 1 and 2  I-line panel cover.

Product Line:
Panelboard

Environment:
I-Line Panelboard Accessories

Cause:
N/A

Resolution:
It is the LP9500 which is obsolete. The the replacement clamp is LP9501 per the Supplemental Digest.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings