Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the life expectancy of the NEMA rated Type S contactors?
Issue:
Identifying life cycle of a NEMA Type S device

Product Line:
NEMA Contactors and Starters

Environment:
Type S contactors and starters

Cause:
Identifying life expectancy of a NEMA device

Resolution:
The life expectancy is based on the NEMA size of the device as follows:

NEMA Size - Mechanical Operations - Electrical Operations
00 - 6,000,000 - 600,000
0 - 10,000,000 - 1,000,000
1 - 10,000,000 - 1,000,000
2 - 10,000,000 - 1,000.000
3 - 5,000,000 - 500,000
4 - 3,000,000 - 300,000
5 - 2,000,000 - 200,000
6 - 1,500,000 - 150,000
7 - 500,000 - 50,000

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings