Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the replacement front safety cover that slips over the contact actuator on the Tesys D-Line contactors and relays?
Issue:
What is the part number for the safety covers for D line contactors

Product Line:
D-Line IEC contactors

Environment:
IEC Contactors  sold and used in the United States

Cause:
Requirement safety covers

Resolution:
The replacement depends on contactor used; select from below:

For LC1D09 - LC1D38, as well as CAD relays, order LAD9ET1
For LC1DT20 - LC1DT40, order LAD9ET1
For LC1D098 - LC1D258, order LAD9ET1
For LC1D40 - LC1D65, order LAD9ET2.
For LC1D40004 - LC1D65008, order LAD9ET2.
For LP1D65004 - LP1D65008, order LAD9ET2
For LC1D80 - LC1D95, order LAD9ET3.
For LP1D80004 - LC1D80008, order LAD9ET3.
For LC1D80004 - LC1D80008, order LAD9ET3.
For LC1D115 - LC1D150004, order LAD9ET4.


For specific machine safety applications we also have red covers:
LAD9ET1S for 9A to 65A contactors.
LAD9ET3S for 80A to 95A contactors.
LAD9ET4S for 110A to 150A contactors.
There are also auxillary contacts available for front mount with a ref cover, model LADN22S, 2NO + 2NC


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings