Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the clear internal operating lever available for the 2510 Type M manual starters?
Issue:
What is the part number for the internal lexan lever on a 2510MCR3 manual starter?

Product Line:
NEMA Contactors and Starters

Environment:
NEMA Manual motor starter, 2510M, 2510T

Cause:
Clear internal operating lever for 2510M needs to be replaced

Resolution:
Yes, order part number 9998 IL1. This internal lever is found only in the NEMA Type 4 Series A & B, NEMA type 12 Series A & B, NEMA 4X, and NEMA 7 & 9 cast iron enclosures.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings