How can we help you today?

What is the Operating Temperature for 9001BW Pendant Stations?

Issue:
Operating temperature for BW pendant stations

Product Line:
Pendant Stations

Environment:
Class 9001 Type Bw Pendant Stations

Resolution:
-13 degree F to +140 degree F
-25 degree C to +60 degree C