Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What auxiliary contacts are provided as standard on Class 8736 Type SE__, SF__, SG__, SH__ or SJ__ NEMA size 3 through 7 reversing starters?
Issue:
What auxiliary contacts can be found in a NEMA Starter sizes 3-7?

Product Line:
Starters, Type S

Environment:
Type S Reversing Full Voltage Contactors and Starters

Resolution:
There is 1 normally closed (9999SX7) auxiliary contact located in the lower right hand corner of each contactor wired from the factory for electrical interlocking purposes. There is also a normally open (9999SX6) auxiliary contact located in the upper left hand corner of each contactor for holding (seal in) circuit purposes.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings