Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the catalog number for 1 normally open or normally closed front mount auxiliary contact for use with GV2 Type M__, Type ME__ or Type P__ manual motor starters?
Issue:
Front mounted 1 no 1 nc aux contact for GV2 Manual Starters

Product Line:
Contactors and Starters - IEC

Environment:
Tesys GV Manual Starter and Protectors

Resolution:
GVAE1, front mount auxiliary contact that can installed to be either normally open or normally closed.
Note: The front mount auxiliary cannot be used with the GV2P__ when the GV2GH7 incoming line insulator is used.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings