Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What ground fault breakers offer people protection (4-6 mA)?
Issue:
Is there a (4-6 mA) ground fault breaker (GFI) breaker for a 480Y/277 V system?

Product Line:
Residential circuit breakers

Resolution:
ONLY QO/QOB and HOM breakers offer GFCI people protection and they are ONLY rated for use on 120/240 Vac circuits. No breakers are available at 277 Vac or above for people protection.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings