Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you determine if 8536SGO_ is Series A or Series B?
Issue:
Determining series of starter for selection of replacement parts

Product Line:
NEMA Starters

Environment:
Products sold and used in the United States

Cause:
Determining series of a NEMA size 5 starter

Resolution:
There are several ways to determine this:
(1) The open style device nameplate should have a series designation.
(2) Series A coils are marked 31096-400-__ where series B coils are marked 31096-320-__.
(4) Series A armature assembly is painted black and is stamped with number ``5`` where series B armature is painted gray and is stamped with the letter ``E``.

Note: DO NOT mix and match Series A and Series B power plant components.

The armature for series A is black and is marked with a Id number ``5``. The armature for series B is grey and is marked with a Id letter ``E``

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings